2022-07-13 7:47 AM
Dual drive support was removed from the MCSDK when version 5.Y.0 was introduced. The release notes for MCSDK V6.0.0 states:
"Dual drive is no more supported at the moment. Support for this feature will be reintroduced in a future release of the SDK"
Is there any information as to when dual drive support will be reintroduced?
/Sune
2022-08-26 5:01 AM
Hi STM
Do you have more information about, when the dual drive feature will be supported again. Will it be at the next release in 2022?
We will appreciate to get an indication of the timeline because we are facing an important hardware decision? Do we need to use one or two STM32 MCU´s to control two BLDC´s?
Best Regards
Thomas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.