2025-09-15 12:10 AM - last edited on 2025-09-15 6:59 AM by Saket_Om
I want to enable the UART communication in MCSDK software which is very time critical task, i enabled UART with DMA, the problem is it cannot transmit more than 2 bytes even if i give 3 or more for transmission
HAL_UART_Transmit_DMA(&huart3, buffer, 3);
I get the call back
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
uartransmissioncomplete = true;
}
after every 2 bytes.
I tested the same program only with UART it works fine transferring more bytes. So, can i just go ahead with transmitting 2 bytes for every call back function, or will i really be able to transfer more bytes in the complete project, since i don't want to disturb the main functionality, i want UART data for data logging.
2025-09-15 7:05 AM
Hello @STuser2
@STuser2 wrote:I tested the same program only with UART it works fine transferring more bytes.
You mean UART without DMA?
Please refer to the example below:
Projects/NUCLEO-G474RE/Examples/UART/UART_TwoBoards_ComDMA
2025-09-15 8:28 PM
You mean UART without DMA?
It is UART with DMA. I have programmed only UART and DMA to see if it works without the integration with motor control.
When i integrate with the main program of motor control, there are so many other high priority interrupts running i am not sure how do i code the UART so that it does not get blocked, only question is why do i get a callback without transmitting all the bytes.
2025-09-16 1:55 AM
Hello @STuser2
Could you please share your code so that we can assist you more effectively?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.