2023-08-10 8:24 AM
I have PM-SMPSM motor that I'm trying to get to spin with the STSPIN3201 - I seem to be able to configure the project in the MC workbench, generate code, and load it onto the micro through CubeIDE just fine - but no matter what I do, the motor moves slightly when I try to spin it up, and the rotor locks in a fixed position. More specifically, it seems to on first boot do a search to determine the encoder/winding relationship by doing a short ramp, but then it does the rotor lock every time I request a speed. The rotor isn't locking in a fixed position, but it seems to be cogging to one of several fixed positions and locking there. Things I have tried:
A few other things that are possibly relevant:
Motor top speed is 4500 RPM, and our max application speed is 2600. I am attempting to spin it at 1300, which is a typical speed for our application.
I am running this in SPEED mode, since POSITION mode doesn't fit in memory without resorting to changing optimization, disabling the UART, etc.
I'm sure the fact that the motor is completely fixed in place is a clue - typically this is a bad commutation sequence or a loose connection or something, but I have checked these things as best I can and don't have an answer so far.
Any thoughts would be helpful,
-R
Solved! Go to Solution.
2023-08-10 9:17 AM
In going over my parameters to provide additional information, I have realized my mistake. I had the quadrature encoder set for 4096 PPR which was not true. It was 4096 COUNTS per rev, but that's 1024 Pulses per rev.
Everything works a treat now. Sorry for the noise on the forum!
2023-08-10 9:17 AM
In going over my parameters to provide additional information, I have realized my mistake. I had the quadrature encoder set for 4096 PPR which was not true. It was 4096 COUNTS per rev, but that's 1024 Pulses per rev.
Everything works a treat now. Sorry for the noise on the forum!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.