2023-11-28 8:41 AM
Hi,
We are using MCSDK_v5.Y.4.
We would like to implement Stall Detection and are considering using the measured iq current (used in FOC) for detecting a motor stall. We intend to use a Stall_Detection_Threshold, which is just below the "Current_Limit" to detect when the iq current exceeds this threshold for a given duration of time: stall_time.
We would like to know if the following function, TSK_MF_StopProcessing(), is recommended to use for stopping the motor,
/**
* @brief Performs stop process and update the state machine.This function
* shall be called only during medium frequency task
*/
void TSK_MF_StopProcessing( MCI_Handle_t * pHandle, uint8_t motor)
{
#ifdef REV_1
R3_2_SwitchOffPWM(pwmcHandle[motor]);
#else
ICS_SwitchOffPWM(pwmcHandle[motor]);
#endif
FOC_Clear(motor);
MPM_Clear((MotorPowMeas_Handle_t*) pMPM[motor]);
TSK_SetStopPermanencyTimeM1(STOPPERMANENCY_TICKS);
Mci[motor].State = STOP;
return;
}
or is there a more immediate "process" or function to use to stop the motor.
From the description in the code, "the MCI_StopMotor() command is used just to begin the
stop motor procedure moving the state to ANY_STOP ".
Thanks and Best wishes,
Jocelyn
Solved! Go to Solution.
2023-11-29 12:30 AM
Hello jocelync2,
Despite what you said concerning the MCI_StopMotor() command is true, it is nonetheless the safest way (and intended way) to stop a motor. You should have no delay issue and you will be able to easily restart your motor afterwards using the MCI_StartMotor() command.
On a different note, have you tried the latest MCSDK 6.2 version for your project ? It contains many firmware improvement both in stability and performance.
2023-11-29 12:30 AM
Hello jocelync2,
Despite what you said concerning the MCI_StopMotor() command is true, it is nonetheless the safest way (and intended way) to stop a motor. You should have no delay issue and you will be able to easily restart your motor afterwards using the MCI_StartMotor() command.
On a different note, have you tried the latest MCSDK 6.2 version for your project ? It contains many firmware improvement both in stability and performance.
2023-11-29 5:04 AM
Hello Gael,
Thank-you very much for your response and your suggestion to upgrade to MCSDK 6.2.
A further question regarding stopping PMSM motors:
We would like to monitor the angular speed of the PMSM motor: When the speed increases above a given limit, we would like to stop the motor immediately.
Further Question: We were wondering where in the MCSDK_v5.Y.4 code, we should perform this monitoring task and then stop the motor when its angular speed exceeds upper limit. We were thinking of performing this within the function:
FOC_CurrControllerM1(void),
in mc_tasks.c file, specifically, just before the application of the Torque PI_Controller stage. The motivation is to perform this check, in a single location in the code (this monitoring of the speed and possibly stopping the motor), where the implementation is applicable for all modes (STC_TORQUE_MODE , STC_SPEED_MODE).
Would this be a good location to implement the monitoring and subsequently, stopping of the motor? or is there a more appropriate location in the code to perform this?
Thanks-in-advance!
Best wishes,
Jocelyn
2023-11-29 8:02 AM - edited 2023-11-29 8:03 AM
Hello jocelync,
The shaft speed is calculated during the MediumFrequencyTask and not the HighFrequencyTask, so I think it would be better to perform your monitoring around (or inside) the CalcAvrgMecSpeedUnit function at the beginning of the MediumFrequencyTask.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.