2025-05-28 8:13 AM
Hello,
I am trying to get my STM32G4B1C3 ESC working for a brushless rc hobbyist motor with unknown motor parameters. I flashed a generic set of parameters to the device and enabled the motor profiler before flashing so that I could estimate them online.
When I connect to the motor pilot app Everything is detected fine with no faults, but then I click begin profiler and it seems to just stall with a high pitch noise and never gets past 7% complete. I have tried swapping the 3 phases in all combinations with no change in behavior:
Motor details:
Aerosky MC2212-980KV
7 pole pairs with standard surface magnets (outboard)
2025-05-28 8:21 AM
Hello @james farrant,
The A2212 motor is available from MCSDK6.3.1 delivery.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.