2025-05-29 12:35 AM - edited 2025-05-29 12:40 AM
I made customized board based on bg431besc1 board all pin defined are same as original board except I did not placed back emf register . it working well just like original board in Arduino in both open loop as well as closed loop with very smooth speed. But when I ran it in stm32ide it did not run but it debugging and show zero fault zero speed . the code i m using is same code earlier i used for original board both Arduino and stm32ide codes and motor is also same. so tell me what is problem also motor pilot it connect when i upload ide closed loop code when connect by usb but when i on power 24v it show try to configure with show correct port nd connected board. this is my code
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.