2019-12-03 6:37 AM
Hy there,
I would like to ask you, if there is possible to get the basic source code that you are uploading to the STM32G431CB ? I am using it with that basic code, with a MOTOR PROFILER GUI. I am trying to change the motor rotation periodicly (eg. after 3 period the direction of the rotation should change IMMIDIATELY) but with the help of the GUI it changes very slow... I would like to modify the code, I just do not know, which code should I download?
Can you please send me the basic source code for STM32G431CB , motor rotation?
Thank you in advance,
N.
Solved! Go to Solution.
2019-12-04 3:57 AM
Thank you for your help, I find my type of devboard, but I can not build it properly. It misses "motorcontrol.h" file that I can not find anywhere :(
2019-12-17 4:02 AM
Thank you Vincent, now my motor is spinning with the right speed. Can you please explain to me how to control is reserval?
2019-12-18 9:20 AM
Hello,
The speed is signed, if you use the void MCI_ExecSpeedRamp( MCI_Handle_t * pHandle, int16_t hFinalSpeed, uint16_t hDurationms ) function.
Just changing the speed sign will change the direction. But beware of the following note:
* @note A ramp cannot reverse the rotation direction if the Application is using
* sensorless motor control techniques. If the sign of the hFinalSpeed parameter
* differs from that of the current speed, the ramp will not complete and a Speed
* Feedback error (#MC_SPEED_FDBK) will occur when the rotation speed is about to
* reach 0 rpm.
Best regards,
Vincent
PS: @Community member I've asked to have the UM2516 updated as per your recommendations. Cheers, Vincent
2019-12-19 4:23 AM
hello,
and what else could I use? I know if I wtop the motor and change the speed sign than it will rotate to another direction, I just need to change the direction immediately. Is there another function or a method to do it?
Thank you
2021-06-27 9:47 PM
Adding of STM32 Motor Control topic.
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.