2019-11-05 9:42 PM
work bench cannot support stm32g4 2 shunt
any one know why which is different cannot support
2019-11-06 2:38 AM
Our FOC algorithm needs three shunts, even if we sample them two by two, and computing the third one.
(sum of the three is theoretically null).
We do require three shunts because depending on the sector, we do not always sample the same phases.
We do have also Single shunt implementation available.
Hope it helps
Cedric
2019-11-06 3:51 AM
hi cedric
when put current sensor on out put after igbt no need 3 phase only 2 phase ok ia+ib = ic this method workbench have for stm32f303 bout for stm32g4 disable this option
if used sensor on ground must used 3 shunt because in some sector vector igb low side off cannt read current if put current sensor in out put all time in software can calculated phase no have current
2021-06-21 11:12 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.