2020-03-24 3:48 AM
Dear
I am looking to test Nucleo-F401 with Motor driver IHM07-M1 but when stating motor profiler, this nucleo board does not appears in the list of supported board. When reading release not of Motor profiler, F401 should be in the supported board.
Please help
Thanks
2020-03-25 10:10 AM
You are right the Nucleo-F401RE is not available in the Motor profiler.
Anyway if you have the motor datasheet you can start a new project with ST MC Workbench software tool and upload the motor data directly inside.
2020-03-25 12:10 PM
Dear Cristiana, thanks for answer however my motor datasheet is not complete and profiler would be a good way to tune. I ordered F303 Nucleo to check only motor parameters. Thanks for your help.
2021-06-27 9:40 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.