2018-04-09 4:26 AM
Does the ST MC FOC lib send an asynchronous message over UART in the event of a fault?
Typically the scenario is that the MCU running the ST MC FOC lib v4.3 detects a fault condition such as over voltage, will it notify the the master (typically PC or other MCU) by sending a message over UART?
Or, do you have to poll the status from master by sending ST Motor Control Protocol message?
#fault-handling #communication2021-06-27 9:08 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.