2018-04-17 8:25 AM
What are the use of the Power Measurement classes in the ST MC FOC lib v4.3?
From the confidential distribution the following classes are part of MC Library module:
MotorPowerMeasurementClass
PQD_MotorPowerMeasurementClass
There is no info on this in UM1053.
#power-measurement2021-06-27 9:07 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.