2018-05-29 11:47 PM
Hello, I downloaded the latest version of st-motor-control. When I open an example, the software informs me that I am using a newer version and must migrate from 4.3 to 5.0.2. I accept.
Now,
I can open the monitor window and I can control the engine. If I want to modify the configuration and generate it, the software informs me that I can not do it because 'F1 mcus not supported in FW for SDK 5.0'
When I load the example, I have the following information:
App: STMCWB
Time: 05/30/2018 08:38:42Project: NonameFilename: F:\MHK\STM32\STEVAL3201\Noname.logType Time Motor Id Message
UNK 08:06:41 The 'Sensor-less (HFI+Observer)' is not supported in the FW for SDK5.0. All parameters will be disabled.UNK 08:06:41 The 'PFC' is not supported in the FW for SDK5.0. All parameters will be disabled.UNK 08:06:41 The 'LCD' is not supported in the FW for SDK5.0. All parameters will be disabled.UNK 08:06:41 F1 mcus are not supported in the FW for SDK5.0UNK 08:06:41 F2 mcus are not supported in the FW for SDK5.0UNK 08:06:41 STSPIN mcu is not supported in the FW for SDK5.0Where can I find an sDK vesion 4.3 ?
Thank.
Christian
2018-06-11 3:57 AM
Dear Christian,
STSPIN3201 and 3202 are now back in the MCSDK 5.1.1 that is available for download.
Regards
Cedric
2021-06-15 1:28 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.