2026-02-10 10:56 PM - edited 2026-02-11 5:27 AM
During Startup,
after
MX_NVIC_Init();
when it jumps into
/* USER CODE BEGIN 2 */
The code is interrupted by
TIMx_UP_M1_IRQHandler()
in its routine,
(void)R3_2_TIMx_UP_IRQHandler(&PWM_Handle_M1);
the code gets stuck at
/* We can not change OPAMP source if ADC acquisition is ongoing (Dual motor with internal opamp use case) */
while (0x0u != pHandle->pParams_str->ADCDataReg1[pHandle->_Super.Sector]->JSQR)
{
/* Nothing to do */
}I'm not able to understand why this is happening. I have not initialized any custom ADC (RCM) yet.
Everything that has run, until that point is generated code only.
With some research I have understood that the TIM1 update routine is infinitely waiting for the ADC(Injected Conversion) to finish.
Is this some kind of race condition ?
This doesn't happen always on every boot/startup. Only randomly, some times.
If it does not crash at this point, I have not observed it to crash at a later point of time.
Am I supposed to something differently in this version of sdk ?
At least, how can I work around this temporarily ?
I upgraded to 6.4.1 from 6.2.1 , and I started facing this.
ST 'SPIN' package G4 - custom board
Single Motor Drive , 3 shunt config.
@cedric H @Fabrice LOUBEYRE
Solved! Go to Solution.
2026-02-19 11:54 PM
@GMA ,
I did try what you suggested. I still saw random occurrences of these crashes.
I spent some time trying to find out what's up.
I found a workaround for this,
LL_TIM_DisableCounter(TIM1);
LL_TIM_ClearFlag_UPDATE(TIM1);
LL_TIM_ClearFlag_CC1(TIM1);
LL_TIM_ClearFlag_CC2(TIM1);
LL_TIM_ClearFlag_CC3(TIM1);
LL_TIM_ClearFlag_CC4(TIM1);
NVIC_ClearPendingIRQ(TIM1_UP_TIM16_IRQn);
//probes
tim_running = TIM1->CR1 & TIM_CR1_CEN;
tim_uif = TIM1->SR & TIM_SR_UIF;
adc1_jsqr = ADC1->JSQR;
adc2_jsqr = ADC2->JSQR;
adc1_busy = LL_ADC_IsActiveFlag_JEOS(ADC1);Since the motor isn't running,
I disabled the timer, cleared flags, irq before enabling TIM1 IRQ
Then started the timer right after that.
// NVIC BLOCK
HAL_NVIC_SetPriority(TIM1_UP_TIM16_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn);
//Start Timer
LL_TIM_EnableCounter(TIM1);I was able to start the MCU over and over without it crashing in the while(ADC->JSQR){} .
I understand this is not a solution. But I can carry on.
It probably needs a fix in the Middleware.
Thanks for your support, Looking forward to a proper solution.
2026-02-11 1:15 AM
Hello @Muthanna,
Do you have a single or a dual drive configuration?
2026-02-11 1:26 AM - edited 2026-02-11 5:08 AM
Hello @GMA
Single Drive Configuration.
My Design is almost identical to EVSPIN32G4 (3 shunt) only with use of the additional MCU pins
I will update the same in my question.
Thanks for your prompt response, looking forward to solve this with your help.
Here's running part of my main()
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_ADC2_Init();
MX_COMP1_Init();
MX_COMP2_Init();
MX_COMP4_Init();
MX_CORDIC_Init();
MX_DAC3_Init();
MX_I2C3_Init();
MX_OPAMP1_Init();
MX_OPAMP2_Init();
MX_TIM1_Init();
MX_TIM4_Init();
MX_MotorControl_Init();
MX_I2C1_Init();
MX_RTC_Init();
MX_TIM2_Init();
MX_TIM3_Init();
/* Initialize interrupts */
MX_NVIC_Init();
/* USER CODE BEGIN 2 */
HAL_Delay(10); // <------ CRASHES HERE 2026-02-12 8:47 AM
Hello @Muthanna,
Did you try using a default MCSDK project without adding I2C1/RTC/TIM2/TIM3 Ips?
2026-02-19 11:54 PM
@GMA ,
I did try what you suggested. I still saw random occurrences of these crashes.
I spent some time trying to find out what's up.
I found a workaround for this,
LL_TIM_DisableCounter(TIM1);
LL_TIM_ClearFlag_UPDATE(TIM1);
LL_TIM_ClearFlag_CC1(TIM1);
LL_TIM_ClearFlag_CC2(TIM1);
LL_TIM_ClearFlag_CC3(TIM1);
LL_TIM_ClearFlag_CC4(TIM1);
NVIC_ClearPendingIRQ(TIM1_UP_TIM16_IRQn);
//probes
tim_running = TIM1->CR1 & TIM_CR1_CEN;
tim_uif = TIM1->SR & TIM_SR_UIF;
adc1_jsqr = ADC1->JSQR;
adc2_jsqr = ADC2->JSQR;
adc1_busy = LL_ADC_IsActiveFlag_JEOS(ADC1);Since the motor isn't running,
I disabled the timer, cleared flags, irq before enabling TIM1 IRQ
Then started the timer right after that.
// NVIC BLOCK
HAL_NVIC_SetPriority(TIM1_UP_TIM16_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn);
//Start Timer
LL_TIM_EnableCounter(TIM1);I was able to start the MCU over and over without it crashing in the while(ADC->JSQR){} .
I understand this is not a solution. But I can carry on.
It probably needs a fix in the Middleware.
Thanks for your support, Looking forward to a proper solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.