2021-08-27 10:14 AM
Are there software project examples of how to use the PTOOL1V1 without the hall sensors? Also, what programming device should be used for the SWD?
Thank you!
2021-08-30 2:45 AM
Hello,
Today there are no other example than the one using hall sensors. In the futur the MC Workbench will provide a fully configurable 6 steps experience.
The SWD can be used by The STLink V2 or V3. STlink is available as a standalone device, but it comes also with all Nucleo Board. If you have one of them, you can reuse the STLink to flash the PTOOL1V1.
Cedric
2021-08-30 7:39 AM
Thank you for that information! Do you have an idea when the MC Workbench will have the 6 step driving solution?
I believe the ESC002V1 does not use Hall Sensors, however, it uses a PWM input to set speed. Does the MC Workbench allow for the change of this PWM control to a POT control? That would solve my problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.