2017-05-19 2:48 AM
Good morning, I can’t compile my project to use the Motor Control Workbench 4.3 Monitor
I summarize the initial process: Open Workbench, New Project, select Power and control after select NUCLEO-F303RE and STEVAL-IPM05F 3Sh and a my custom motor profile.
Now can Save my project, use this folder:
C:\Program Files (x86)\STMicroelectronics\FOC SDK\v4.3.0\STM32 PMSM FOC LIB\Web
After set all motor, power stage, Drive management and Control Stage parameters, save the project.
Press “generation�? and select the default folder. Now it’s appear a pop-up to remember to program my nucleo. I will use AC6, I open this file:
C:\Program Files (x86)\STMicroelectronics\FOC SDK\v4.3.0\STM32 PMSM FOC LIB\Web\Project\AC6\STM32F30x_UserProject/.project
AC6 start, I will compile but I can select 4 option but none for my STM32F303.
When I try to compile there are a 2 problem:
#error 'Invalid configuration: MCU definition in Control stage parameters.h not compatible with selected board. Please use the ST Motor Control Workbench to configure the firmware according your system.' STM32F30x_UserProject line 88, external location: C:\Data\Software\STM32\Workbench\Web\Project\CrossCheck.h
make: *** [UI Library/src/UserInterfaceClass.o] Error 1 STM32F30x_UserProject
what am I doing wrong?
Thanks
Manuele
2017-10-17 5:49 AM
I am having the same problem only with IAR as IDE. There is no option to select F303RE in the drop-down menu for compilation and download/debug.
There is only:
STM32F30x_UserProject - STM32303C-EVAL_SINGLEDRIVE
STM32F30x_UserProject - STM32303C-EVAL_DUALDRIVE
STM32F302_SINGLEDRRIVE
P-NUCLEO.IHM001_SINGLEDRIVE
2021-06-15 1:53 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.