2017-05-23 10:57 PM
Hello, All:
I use (ST Motor control Workbench) parameters in power management where I set up some flow parameters, and then generate the file in Power stage, But I did not find the parameters.h file to set my parameters, why, where is it?
/*********** Over-current protection section ************/
#define OVERCURR_FEEDBACK_POLARITY EMSTOP2_ACTIVE_LOW #define OVERCURR_PROTECTION_HW_DISABLING DOUT_ACTIVE_HIGH/************************************************* ************/
There is no parameter about overcurrent.
Thank you!
2021-06-27 6:39 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.