2021-09-27 10:55 AM
Ian using a dyno to apply load and using B-G431B-ESC1 with a pmsm motor
SPEED: KI= 950, KP= 13767, Torque KI= 1005 reduced from 3005 earlier torque kp=82 (tuned settings)
I have attached a snapshot ,as gradually I increase load (oz-in) in steps
1) at rpm <1500 I am able to track the curve with increased load in const rpm
2) At rpm >2000 ,at higher load region the speed oscillates heavily (see snapshot attached)
I have attached the datasheet of motor from which it is clearly visible that upto 2880 RPM it can take continueous load torque of 39 oz-in
Could you suggest what could be the problem?
2021-10-20 5:36 AM
Dear @Ajosh.1
Welcome to the STM32 Community
Sorry for late answer.
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.