2023-06-08 4:55 AM
I'm using motor profiler for the motor control. I have the following hardware components:
In the motor profiler, it mentions that IHM16M1 can only work sith STM32 Nucleo-G4 and that F4 and IHM16 combined is not supported.
Is there a workaround available to test the motor despite this limitation?"
Solved! Go to Solution.
2023-06-08 5:26 AM
Hello @GJamo.1,
Which version of the MCSDK do you use?
I just checked with the MCSDK 6.1.2, and the combinaison Nucleo-F4446RE+X-NUCLEO-IHM16M1 is proposed by the profiler.
Regards
Cedric
2023-06-08 5:26 AM
Hello @GJamo.1,
Which version of the MCSDK do you use?
I just checked with the MCSDK 6.1.2, and the combinaison Nucleo-F4446RE+X-NUCLEO-IHM16M1 is proposed by the profiler.
Regards
Cedric
2023-06-08 11:27 AM
Thanks for the info
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.