2024-11-25 6:17 AM
Hello
I'm evaluating B-G431B-ES1 design.
As I don't have accurate specifications for the motor, I'm going through motor profiler.
If I use SDK 5.4.8, profiling seems to work. At least, the motor turns.
If I use SDK 6.3.2, profiling whistles while keeping the "startup beep-beep" but the motor never starts. Before that, I built a firmware with the motor profile option activated.
What did I miss?
Thanks
Julien
Solved! Go to Solution.
2024-11-28 10:05 AM
Test 1:
- I removed esc feature.
- opened motorpilot
- loaded gui SimpleAppMCPV2.qml
- error -> this gui does not support motor profiling app (something like this).
- removed motor profiler from "application configuration" tab
- restart gui.
- motor runs smoothly.
Is it what you requested?
Test 2:
- no motor profiler in app configuration
- esc enabled
- potentiometer enabled
-> with this configuration, the motor does not start with the button, whatever the position on the potentiometer.
2024-12-03 12:47 AM
Hello @JulienD,
Test1: yes.
Test2: if you want to use Potentiometer feature, only select Potentiometer feature and disable ESC.
It is not possible to control speed with both feature (ESC and Potentiometer) at the same time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.