2024-12-03 1:01 AM
For steval esc001v1 with MC workbench Version: 6.3.0, to run firmware do we need any other connections other than below mentioned because motor is not running?
Connection:
12V DC input
SWD connections with STLink
3 phase motor wire connection at OUT1,2,3.
Firmware:(inside main())
MC_ProgramSpeedRampMotor1(RPM_2_SPEED_UNIT(600), 2000);
MC_StartMotor1();
HAL_Delay(4000);
MC_StopMotor1();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.