2025-06-25 8:26 AM
Hello, I have a custom Board based on the EVSPING4 Dual. I was able to flash the code and Debug with a segger j-link. I added a Uart message after the init and I could see the message with putty. But when I try to connect with motor Pilot the error No STlink connectet pops up. I generated the code with motor control workbench and enabled motor control. In the code the uart is initialized but i cant find any code to actually communicate an control the motors over uart.
Thanks
Solved! Go to Solution.
2025-06-25 2:17 PM
Changing the GUI worked
2025-06-25 2:04 PM
I found the USART1_IRQHandler Handler in the code and set a breakpoint in it, when i tried to connect with motor pilot it wasnt triggered, but when I opened putty and typed some characters in it was triggered
2025-06-25 2:17 PM
Changing the GUI worked
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.