2016-10-24 10:53 PM
Hi,
hardware for running bldc motor at 800 rpm in sensorless foc mode at 110V..
I have followed the below steps...
1 Downloaded ST Motor control workbench 4.2
2 Downloaded IAR embedded workbench
3 Project created in Motor control workbench as per Table 1 provided in UM1697 user manual for STEVAL-IHM038V1 document
4 The generated header files are copies to System Parameter folder
5 Project is created by referring section 9.1 in UM1052 document
6 STM32F10X Example workspace with simple time base is selected
7 The project configuration STM32100B EVAL is utilised
8 Project is compiling successfully
I have loaded generated hex file on the hardware and trying to run the motor but it is not running
The PWM pins are stuck up at 3.2V
Pl. suggest/ provide some solution to resolve above issue
Regards kaushik
2021-06-27 8:50 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.