2016-09-08 2:19 PM
Hi,
I've been working with MC workbench and want to use a smaller package STM32F303. However, the project configuration for analog inputs only offers pins that are not available on the LQFP48 ''C'' package. I have no wish to use the 64 or 100 pin package for a small simple application. Can I use the STM32F303CB part? Thanks in advance. #stm32f303-mc-workbench2021-06-27 8:51 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.