cancel
Showing results for 
Search instead for 
Did you mean: 

Measuring of torque from STSPIN220 stepper motor driver.

Jeremiah
Associate II

Hi,

I am using a Stepper motor and the motor driver IC used is STSPIN220. I have to measure the torque of the motor to find when it has reached maximum load. What is the best way to do it?

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @Jeremiah,

the STSPIN220 cannot measure the torque of the motor.

The most effective way to measure motor torque and identify the maximum load point is by using a dynamometer.

If you feel a post has answered your question, please click "Accept as Solution"
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.