2023-05-03 12:47 PM
When I try to generate code for a project that was generating properly in Feb 2023, I now get the following errors:
ERROR [LineInfo_to_exitCode.log_LineInfo] The ST intranet updater server is unknown: mcucrossselector.codex.cro.st.com
ERROR [LineInfo_to_exitCode.log_LineInfo] Found unsupported composite condition: CLASS='Data Exchange' GROUP='STM32_MetaDataManager'
ERROR [LineInfo_to_exitCode.log_LineInfo] Found unsupported composite condition: GROUP='STM32_MetaDataManager' CLASS='Data Exchange'
I'm using
MC WorkBench: 5.4.8.21553
WB_to_MX : : 1.5.1.template-21-11-15
STM32CubeMX: 6.4.0
MC Firmware Library: 5.4.8
Generation Options:
Target Toolchain: ST STM32CubeIDe
Target Driver : LL-Low Level
Target STM32 FW: 1.5.0
The project is a G081B eval board with a IPMnM2S 3-shunt power stage
I've now Updated my
MC Workench to the latest : 6.6.1
STM32CubeMX to : 6.8.1
STM32CubeIDE to 1.12.1
MC WorkBench: 6.6.1
WB_to_MX : : 6.1.0.template-22-12-05
STM32CubeMX: 6.8.1
MC Firmware Library: 6.1.1-Full5.4.8
Generation Options:
Target Toolchain: ST STM32CubeIDe
Target Driver : LL-Low Level
Target STM32 FW: 1.6.1
Using CubeMX 6.8.1 instead of 6.4.0 got rid of the first error (unknown: mcucrossselector.codex.cro.st.com)
But the other errors remains
ERROR [LineInfo_to_exitCode.log_LineInfo] Found unsupported composite condition: CLASS='Data Exchange' GROUP='STM32_MetaDataManager'
ERROR [LineInfo_to_exitCode.log_LineInfo] Found unsupported composite condition: GROUP='STM32_MetaDataManager' CLASS='Data Exchange'
Any suggestions greatly appreciated.
Thanks!
Best Regards
Solved! Go to Solution.
2023-06-07 1:14 AM
hello, did you flash the FOC project correctly? if the Motor Pilot tells you that it is a 6-Steps project, you have not flashed the correct project, because they are different.
the project creation problem you indicate does not affect the generation of a functional Motor Control project
2023-06-07 1:16 AM
Hello, the problem that is displayed is not a blocking problem, it is simply related to an update feature of Cube Mx, it does not impact the generation of a Motor Control project, so you can ignore the problem .
2023-06-07 9:53 AM
When I going back, trying to run the profiler, I have to flash the NUCLEO-G431RB#X-NUCLEO-IHM08M13Sh#(6.1.2).hex manually.
But when I am running the Pilot, it seems to flash something else that I dont have control over. Or do I?
Pls. let meg know.
I am alsways using the NUCLEO-G431RB and either use a IHM08M1 modified to 3Sh or the other original/unmodified IHM08M1 1Sh (for six-step
Rgs
Steinar
2023-06-08 7:48 AM
I added the .properties file and still get exactly the same errors :
2023-06-08 15:26:25,076 ERROR
[LineInfo_to_exitCode.log_LineInfo]
Found unsupported composite condition: GROUP='STM32_MetaDataManager' CLASS='Data Exchange'
2023-06-08 15:26:25,078 ERROR
[LineInfo_to_exitCode.log_LineInfo]
Found unsupported composite condition: GROUP='STM32_MetaDataManager' CLASS='Data Exchange'
Zied, may I ask, is there something strange about the double quote marks " in your proposed .properties text?. Both fault description lines seem to start with a " but not end with one. I edited the file to add those " but still errors are the same so I restored them to your original.
I am not sure where to go from here. Any ideas please?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.