2024-06-24 2:59 AM
Hello. Trying to profile one of my engines with the ST Motor Pilot Tool (profiler) V1.2.9. Without any success.
I have seen this warning in the STM32 Motor Control FAQ section.
The STM32 MC motor profiler has the following limitation: it cannot profile motors with Rs < 1 Ω or Ls < 1 mH.
If you still face problems, profile your motor manually using the following procedure.
Since my engine met these characteristics.
I have calculated the electrical parameters of the motor following this tutorial and also the tektronix application note (Capacitance and Inductance
Measurements Using an Oscilloscope
and a Function Generator).
Now I would like to be able to use the engine profiler to obtain the mechanical parameters of the engine.
Can it be done somehow with the profiler or can i calculate ir manually?
Thank you so much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.