2024-09-09 12:24 AM - edited 2024-09-09 12:30 AM
Dear All,
My platform as list:
Control Board: B-G473E-ZEST1S
Power Board: STEVAL-LVLP01
Motor: B-MOTOR-PMSMA1
Platform: MCSDC 6.3.0, (I attached my Workbench configuration file as follow)
CubeIDE: 1.15.1
When I try to evaluate the HSO, the Motor pilot appear in weird value.
The speed reference and mechanical speed is wrong.
Also, there are a orange waring, "Access Register of Bus Voltage resulted in error" on the buttom.
Once I start the contol, it will occurs "Over Current Fault"
Has anyone encountered a similar issue? How can it be resolved?
Best Regards,
2024-09-09 12:56 AM
Hi,
In fact you are trying to use STOPLL/Cordic UI with a HSO firmware.
Please load the MC_FOC_ZEST.qml UI instead.
Thanks
BRs
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.