2023-03-28 6:08 AM
Hello,
I'm using bldc motor. Battery Voltage is 40.4V. I run the motor on no load the battery voltage is 40.4V and when I apply the load the voltage is dropping.
load(current) is 1A & voltage is 40.3V
load(current) is 2A & voltage is 40.2V
load(current) is 3A & voltage is 40.1V
load(current) is 4A & voltage is 39.9V
how to slove this problem if any one know help me.
2023-03-29 12:25 AM
our System Design,
I'm working on EV Two wheeler Cluster. I measure the voltage from battery using voltage divider method.
the battery voltage (31 - 40.5) is convert into battery percentage(0 - 99).
In driving time, the voltage is dropping depends on the load. the load is 4A that time the battery is 20 percentage decreas. this is affect the SOC.
2023-03-29 3:04 AM
For a really good evaluation of battery charge status, you need more than the voltage.
At least know the capacity (Wh), constantly measure voltage and current over time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.