2020-11-20 9:08 PM
i am confused how to write a code to drive the stepper motor selecting the 2 timers with interrupt method. By setting one timer = 100khz, and another timer = 3khz. i need to display one pulse after 33 counts each on my oscilloscope. can you please help me with it. I have displayed some code below. can you please say me the mistakes i have done and what i need to add to it to work.
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == htim2.Instance) //100KHZ
{
pulse_count =__HAL_TIM_GET_COUNTER(&htim2);
if(pulse_count == 33)
{
HAL_GPIO_WritePin(GPIOA, dir_Pin, GPIO_PIN_SET); //pin PA3
for(int i=1; i<=300; i++)
{
HAL_GPIO_WritePin(GPIOA, step_Pin, GPIO_PIN_SET); //pin PA4
HAL_Delay(0.1);
HAL_GPIO_WritePin(GPIOA, step_Pin, GPIO_PIN_RESET); //pin PA4
HAL_Delay(0.1);
}
//HAL_Delay(500);
HAL_GPIO_WritePin(GPIOA, dir_Pin, GPIO_PIN_RESET); // anticlockwise
for(int i=1; i<=300; i++)
{
HAL_GPIO_WritePin(GPIOA, step_Pin, GPIO_PIN_SET); //pin PA4
HAL_Delay(0.1);
HAL_GPIO_WritePin(GPIOA, step_Pin, GPIO_PIN_RESET); //pin PA4
HAL_Delay(0.1);
}
pulse_count=0;
}
pulse_count++;
}
}
Thank you
2020-11-21 9:48 AM
I don't read your code thoroughly, but I have some remarks:
HAL_TIM_PeriodElapsed() is called from ISR, so it have to be very short.
Waiting should not be used in an ISR: do not use HAL_Delay() in ISR.
HAL_Delay() argument is milli-seconds expressed as uint32_t. If you use HAL_Delay(0.1) I think the delay will be 0.
You don't say what doesn't work...
2020-11-21 12:38 PM
Nikita91 is right!
HAL_Delay() is not precise for arguments less than 1, use the timer of a for loop, though as Nikita91 says, it is better not to use delays in ISR. another thing is that, as I can recall, for stepper motor you should turn on and off four coils, I only see one pin in your code, and yes, what doesn't work?
2020-11-22 7:51 PM
i am not able to drive my motor . if i debug and run my code i am not able to drive my motor. can you say me the reason why the motor is not rotating please.
Thank you
2020-11-22 7:54 PM
i am not able to drive my motor . if i debug and run my code i am not able to drive my motor. can you say me the reason why the motor is not rotating please. As you said i should use four coils to turn on and off but i didn't understand what you mentioned can you say me in detail please.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.