2022-02-14 12:12 PM
2022-03-28 10:27 AM
Hi,
Thanks for your answer.
My solution is that I short-circuit the jumper J1 via a transistor in the error state and thus the gate driver automatically goes into error, since the maximum possible drain-source voltage can be 0 V in this case and an error is therefore triggered directly.
Regards
Bernd
2022-02-16 4:26 AM
Hello @BPfei.1 and welcome to the ST Community.
To achieve the operation you described you could use the break function (BKIN) of timer TIM1.
When activated, the break circuitry shuts down the PWM outputs and forces them to a predefined safe state.
You have two options to associate the TIM1_BKIN function:
- a User Switch: SW1 or SW2
or
- the PA15 GPIO, available on pin 1 of CN5 Arduino connector.
Let me know if these info are useful to you, if yes please "Select as Best" label to close the topic.
2022-03-28 10:27 AM
Hi,
Thanks for your answer.
My solution is that I short-circuit the jumper J1 via a transistor in the error state and thus the gate driver automatically goes into error, since the maximum possible drain-source voltage can be 0 V in this case and an error is therefore triggered directly.
Regards
Bernd
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.