2015-12-20 2:09 AM
Hi,
Does the motor control software suite (STM32 PMSM FOC LIBv4.2) support STM32F401, '411 and '446 processors? When I tried it, it didn't allow another option for CPU clock than 168, and as far as I know the above processors support 84, 100 and 180MHz. (because of the ''advanced'' features that I want to use I seem to be pushed towards the higher end processors, the 4xx series. And a '405 seems overkill to me).2016-01-07 8:41 AM
Ciao Roger
At the moment the F401 and F411 are not supported by the FOC library. Ciao Gigi2016-01-10 8:06 AM
P.S. The forum has a bug: it will not collapse the ''quoted messages'' after an edit of a post.
2021-06-27 10:55 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.