2014-08-08 3:31 AM
Hello,
I would like to use the latest FOC library for small PMSM motor. I'm using STM32F303VCT6 MCU and I would like to use internal PGA. But motor doesn't run at all. Start sequence starts, but with very high current consuption (higher that I set in WB). I finaly fount that probably AD converter doesn't give a correct value. I see it mainly on Vbus voltage measurement. Measured value is not correct. It shoul be ~325V but reading from MCU give me a value ~189V and it fall down to ~21V after few seconds. Voltage on board is corrent, also MCU ADC works correct - I mean nothing is damaged on the board. I've check it with modified example project in StdLib for STM32F3 and it converts value from Vbus pin. So it seems to me, that something is wrong with setting of AD converter in library. ADC does not measure correct values of Vbus and probably also phase currents and that's why motor has during start so big current consuption and doesn't run. I'm attaching my settings in WB. Maybe I sould mention, that I use KEIL MDK to compile library. Any help/tips would be helpfull. Thanks. Daniel #foc-adc #mcu #foc-adc #foc #foc-adc2014-12-20 9:08 AM
thank you very much Daniel sir
2015-01-28 9:03 PM
dear daniel , i have found these error while building my code. i have attached MC WB project and , pic of errors as well. please guide me
thanks ________________ Attachments : basic.stmc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzJO&d=%2Fa%2F0X0000000bJd%2F9xuk9mzr8EiS5gLWZsXXIUYtIkNzqZyZc52IvOYqJQg&asPdf=falseerrors.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzIM&d=%2Fa%2F0X0000000bJe%2FiuNvRNyrLPE9ERyArLxFr9OC7TYxBJ4w_HfHrRYIk.g&asPdf=false2015-02-06 9:45 PM
dear daniel , please tell me whether i have to use batch build or just build for compiling the project? i am using web distribution library not confidential
2015-03-03 7:11 AM
Hello Raza,
I'm sorry but I will not help you with this question. I'm using KEIL not a IAR compiler. I think, you should follow instruction included in library. It doesn't depend on whether you use web or confidential version. Daniel2015-03-05 5:10 AM
kindly tell me where are the insturction in the libraray?
one last question is current sensing feedback is necessary for the pwm generation?because when i download the code into the controller ,no pwm generated at the gpio pins2015-03-12 4:14 AM
You will find instruction in readme file or there is a doc folder with nice pdf file called Quick Start for STM32 PMSM MC Library v4.0.pdf. There you will find a lot of information how to use library. Beside of these, there is a lot of trainings especially for FOC library. As I remember, two years ago I visited one of these trainings. These time it was in Prague in Czech republic. As I remember there were more trainings around the world. Please try to check ST web.
Current measurement is essential for control. Daniel2015-03-13 3:44 AM
2015-03-13 3:45 AM
okay.
but in my country there is no training institutes of stm library.even there is only a small office , that is only for sales of hardware. please can you tell me.. Is there any tutorials (vedios) at any website?2021-06-27 10:50 PM
Adding of "STM32 Motor Control" topic".
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.