2019-10-06 7:21 PM
I am using a B-G432B-ESC1 board and ST Motor Control Workbench to test run a couple of brushless DC motors equipped with Hall Effect sensors. When attached to a motor with Hall Efect sensors, does the Motor Profiler program look at the inputs from the Hall sensors to determine their phase relationship, so automatically configure the signals into the correct timing order through firmware when using the motor with the Motor Control Workbench? Or do the Hall sensor inputs need to be wired to the ESC in a defined order ?
2021-06-21 11:15 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.