2019-07-26 8:20 AM
Hi there, I am using ststem workbench for stm32, cube mx v 5.3 and mcsdk 5.4. I want to develop a dual motor application with stm32f303re. However, after I generate the code and upload it. It cannot connect through the monitor. (Works for single motor). What would be the potential problem? I would be very appreciate and gratful for receiving any of your suggestions.
2019-07-26 9:16 AM
HI for anyone encounter the same problem. I just solved this issue. Before assigning pin in st motor control workbench, please check if the pin really exsist on the chip. If you assign a pin which is doesn't exist, error occurs.
2021-06-22 1:20 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.