2020-07-15 5:09 AM
Hi,
I'm beggining with MCSDK.
I load the example "EvalG474E_3Shunt_IHM23v3_HAL.stmcx" and the dialog box "Analog Input and Protection" configure the Sampling Time to 6.5 ADC clk resulting in 96nS. So the ADC clock is supose to be 6.5/96nS = 67.7MHZ. But the generated code shows ADC selected from PLLP with 42.5MHZ and with Async clock/4, so ADC clk = 42.5/4 = 10.625MHZ.
And the generated code is imcomplete, there's nothing in the main loop, no interrupts, etc.
Is there a complete motor control example for any G4 any driver that works? That I just need to compile and program into the flash.
Solved! Go to Solution.
2020-07-23 8:53 AM
Hello Asantos,
the easiest way will be to use a G4 example from the Example Projects list from the first page of the MCWorkbench.
you can choose: Speed ramp with Potentiometer on P-NUCLEO_IHM003 kit by example (with STM32G431RB inside)
Thanks and best ergards,
Claire
2020-07-23 8:53 AM
Hello Asantos,
the easiest way will be to use a G4 example from the Example Projects list from the first page of the MCWorkbench.
you can choose: Speed ramp with Potentiometer on P-NUCLEO_IHM003 kit by example (with STM32G431RB inside)
Thanks and best ergards,
Claire
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.