STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Resolved! STM32F303 HIGH INJECTION FREQUNCY

HIANY ONE CAN HELP TO ME I NEED ADD LOW SPEED SENSORELESS (HIGH INJECTION FREQUNCY ) TO MY MOTOR CONTROL SOFTWARE FOR PMSM I KNOW MOTOR CONTROL WORK BENCH ST HAVE THIS FUNCTION ANU ONE HOW ONLY ADD THIS LIBRARY AND WHAT IS INPUT OUT ALL CONTROL FOC I...

Resolved! stm32f303 timer1 motor control

when used timer1 for motor control some time need active low side signal in program with hand not follow pwm out put how to do this disable all output timer wait for turn off time set io bit to active mode (reset or set )change pinout timer to out p...

Resolved! Application note

I'm working on a project where I have to drive a brushless motor. I'm using a NUCLEOF302R8 + X-Nucleo IHM08M1 with STM32CubeExpansion_SPN8_V1.0.2. I can't control my engine because I don't know how to modify the parameters contained in the MC_SixStep...

UVagl.1 by Associate II
  • 1808 Views
  • 2 replies
  • 0 kudos

Resolved! STEVAL-SPIN3201 used with Hall sensor AND Encoder

Hello, I try to control a motor using STEVAL-SPIN3201, a hall sensor and a encoder (in position control). I compile the generated files (generated via ST motor control workbench) via make. In speed position based on hall-sensor, the compilation work ...

FGron.1 by Associate II
  • 2123 Views
  • 3 replies
  • 0 kudos

Resolved! BUGREPORT MCSDK 5.4.3 (and temporary fix)

Hi,since a couple of days i tried to get the STEVAL-ROBOT-1 up and running properly. But as i mentioned here:https://community.st.com/s/question/0D53W000003yGcdSAE/to-choice-a-kit-for-pmsmyesterday, i got more problems, than i would have expected fro...

chaaalyy by Senior II
  • 24359 Views
  • 20 replies
  • 4 kudos

Resolved! SiC inverter design - high switching frequency

I am designing a SiC inverter for a Formula SAE student team, using a 72MHz STM32F302CC with the motor control library. The desired switching frequency is 50-100kHz, depending on the device we select. Reading the motor control manual, I discovered th...

Resolved! Software support for the baord EVSPIN32F0251S1

Hello,I would like to build a circuit to drive a three phase BLDC motor and the board EVSPIN32F0251S1 seems to be a choice, but i can't find the software easily. Does anyone know a three phase BLDC firmware project for this board? My build tool is Ke...

WWang.12 by Associate
  • 1289 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.