2025-07-08 10:29 AM
Hello,
I am using the EVLSERVO1 board and trying to monitor the DAC outputs with an oscilloscope, since the high-frequency plots in Motor Pilot are difficult to use effectively. I enabled DAC Debug in the FOC Wizard, assigning DAC Out 1 to PA4 and DAC Out 2 to PA5. After doing this, I checked CubeMX and confirmed that these pins are configured correctly.
According to the EVLSERVO1 schematic, it looks like I should be able to connect the oscilloscope probes to pins 8 and 5 on the J2 connector. However, when I select a variable to output to the DACs from within Motor Pilot, I see no signal on the scope, just noise.
Is there anything else I need to configure to get the DAC output working?
Thanks
2025-07-09 8:05 AM
2025-07-09 9:07 AM
2025-07-16 2:46 AM
Hello Isaac,
Thank you for your question. Could you please elaborate on the reasons you think the MotorPilot is difficult to use ? We are always looking for any way our tools can be improved and your feedback is important to us.
Concerning your DAC issues, may I know the what kind of variable did you try ? Was it currents, speeds ? Is the behaviour the same every time ? Also, what kind of motor are you trying to run ?
Depending on your answer, know that this may very well be a simple scaling issue.
Let's say for example that your motor is 2Amp rated, and you want to have a look at the currents through the DAC. Knowing the EVLSERVO1 board can measure from -165A to 165A, the DAC output will be very close to 1,65V. (1.65 + 2/330*3.3 = 1.67V)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.