2024-06-17 1:39 PM
Hi,
I'm using STM32G432RB Nucleo board with X-NUCLEO-IHM16M1, and connecting a 3-phase DCBL motor (RaceStart BR2205, which requests 7.4V - 14.8V).
Followed with the instructions in UM2415. I used a power supply with 12V/2A on X-NUCLEO-IHM16M1.
D1 EN/FAULT LED is always red, and D8/9/10, Motor Phase LEDs are never turned On, before or after I pressed the Blue Button (Start/Stop Motor) (on STM32G432RB Nucleo board).
Here is how I generated the code:
MC Workbench 6.3.0, FOC/3 Shunt
STM32CubeMX 6.10.0, STM32Cube FW_G4 V1.5.2
MDK-ARM V5.32
No error in each of these steps of the project and the code generation.
When I pressed the Blue Button (Start Motor) (on STM32G432RB Nucleo board), I saw PC13 (Start/Stop pin) generated a pulse.
Am I missing anything in the setup?
Solved! Go to Solution.
2024-07-19 12:36 AM
Hello @Texram,
In UM2415, in "4.1 Operation mode and sensing topology selection" chapter, a table describes needed HW configuration for 3Shunt topology, are you aligned on this?
Does your boards are coming from IHM03 kit? If yes, could you check that, with Gimbal motor and FW project example available in motor control workbench as "Speed ramp with Potentiometer on P-NUCLEO-IHM003 kit", boards are functional?
2024-07-19 12:36 AM
Hello @Texram,
In UM2415, in "4.1 Operation mode and sensing topology selection" chapter, a table describes needed HW configuration for 3Shunt topology, are you aligned on this?
Does your boards are coming from IHM03 kit? If yes, could you check that, with Gimbal motor and FW project example available in motor control workbench as "Speed ramp with Potentiometer on P-NUCLEO-IHM003 kit", boards are functional?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.