STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

where to find the define data

Hello,Now I am refer to a design of NUCLEO-G474RE board for Motor Control with 6 step method. I found there are some define data of TIM setting. but I cannot get the value of the define data. could you tell me where to find the defined data?Thanks!dq...

dqsh06_0-1721643468493.png dqsh06_1-1721643520966.png
dqsh06 by Senior
  • 2917 Views
  • 5 replies
  • 0 kudos

Motor Pilot and Plot

Hi,I'm using MC WB 6.3.0 with Motor Pilot.I wonder how to plot the following signals that are defined in MC WB in Motor Pilot:PWM_CHU_H, PWM_CHV_H, PWM_CHV_H,BEMF_U, BEMF_V, BEMF_W  I don't see these registers are defined in the list of Registers in ...

Texram_0-1721086176101.png
Texram by Associate III
  • 2211 Views
  • 2 replies
  • 0 kudos

adafruit drv8833 with NUCELO-L432KC

Hello everyone, I'm new to STM32 world, trying to run a 5 dc motor with adafruit drv8833 and NUCELO-L432KCI connected it as belowNUCELO-L432KC a0 > ain1NUCELO-L432KC a1 > ain2NUCELO-L432KC vin > vmNUCELO-L432KC gnd > gnddrv8833 aout1 > motordrv8833 a...

Operating BLDC motor in Speed Control Mode

Hello!We are trying to run the BLDC Motor (BL34E34-01) in speed control.A project was previously shared with us that allowed us to run the same motor in position control mode. Given a target position and duration, the motor reaches the final position...

JAM_1999 by Associate
  • 1542 Views
  • 1 replies
  • 0 kudos

Resolved! D1 LED Red on X-NUCLEO-IHM16M1

Hi,I'm using STM32G432RB Nucleo board with X-NUCLEO-IHM16M1, and connecting a 3-phase DCBL motor (RaceStart BR2205, which requests 7.4V - 14.8V).Followed with the instructions in UM2415. I used a power supply with 12V/2A on X-NUCLEO-IHM16M1.D1 EN/FAU...

Texram_0-1718656756187.png
Texram by Associate III
  • 1395 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.