2020-05-27 7:57 AM
Hello,
i want to use the function MC_GetPhaseCurrentAmplitudeMotor1() from the Motor Control SDK to get the true current of the motor.
I used the following formula to calculate the current, but I didn't get the proper value.
uint16_t IS16A = MC_GetPhaseCurrentAmplitudeMotor1();
float current = ( IS16 A * VDD ) / ( 65536 * RSHUNT * AMPLIFICATION_GAIN );
where
VDD is 3.3 V
RSHUNT is 0.01
and AMPLIFICATION_GAIN is 12.6
2020-09-11 6:33 AM
Dear TKlei.5
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-16 2:52 AM
Yes.
2020-10-14 8:51 AM
Dear @TKlei.5
Could you give more details to the STM32 Community about the material you use (HW and SW, tools and versions, board(s), motor(s) and so on)?
Best regards
Laurent Ca...
2020-10-26 2:49 AM
Dear @TKlei.5
Any news?
Best regards
Laurent Ca...
2020-11-02 12:20 AM
Dear @TKlei.5
As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...
2020-11-25 11:48 PM
Hi i am having same problem
I am using evspin32f0602 single shut board
I want to display motor amp but I am not able to get the value
2021-03-10 9:24 PM
Dear @Fkadr.1
This is a fairly old (and closed) post.
If you encounter the same issue, please open a new question referring to this post,
otherwise the community will not see your question as it appears here.
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.