2022-08-14 7:30 AM
My setup:
NUCLEO-F446RE and STEVAL-IPM15B
"ST Motor Control Workbench" "Power Stage - Current Sensing" settings:
These values are in "power_stage_parameters.h" too.
However, Motor Pilot in "Rev-up" tab, "Phases configuration" -> click "Read all", reads as follows:
That effectively lowers down current/torque about 30% in rev-up phase.
Is it a bug or a feature? Motor Pilot does not read RShunt and gain values from the firmware?
Thank you.
2022-08-25 5:20 AM
Hello,
"Read all" corresponds to full fill the "Phase configuration" table only. If you want to display the table in "Amp" format and not in "S16A" format, you have to enter manually the "Rshunt" box values in order to have a correct conversion.
Best regards.
GMA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.