2023-07-18 8:44 PM
I would like to have precise, slow motion control of a BLDC motor from a hoverboard. This 1 minute video shows it well: https://www.youtube.com/watch?v=JMXz5tzpq7U
Would a "STEVAL-SPIN3202" do this?
Many thanks
Marc
2023-10-28 1:59 PM
I two would like to know if I can use the motor control software out of the box to do this or if I should start looking at simpleFOC and how I could port that work to my project.
2023-10-31 8:00 AM
Hello MarcF,
First of all, we would like to apologize for the delay in replying to your post.
Concerning your issue, if it is still relevant, I have looked at the video you posted, and dug a bit further in the project of the publisher. It appears that what you are seeing on the one-minute long video is in fact an Open Loop system. The MCSDK provides an Open Loop solution that can be implemented on the STEVAL-SPIN3202.
However, if you are searching for a Closed Loop, Low Speed, Sensorless Motor Control, I am afraid the STEVAL-SPIN3202 is not powerful enough for such a task.
I advise you to use an encoder to get your motor position in that case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.