STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

how to calculte B-EMF constant from torch constant

Hi, I'm working with an Maxon 3-phase 1-pole BLDC motor, following is it's motor data table or attached file. the colum with red rectangle is the motor type we're now dealing with.I wondering how can we get the B-EMF constant in the MC workbench elec...

motor param 24V.png params.png
jflash by Associate II
  • 4826 Views
  • 4 replies
  • 0 kudos

BLDC motor driver

I would like to have precise, slow motion control of a BLDC motor from a hoverboard.  This 1 minute video shows it well:  https://www.youtube.com/watch?v=JMXz5tzpq7UWould a "STEVAL-SPIN3202" do this?Many thanksMarc

MarcF by Associate
  • 2272 Views
  • 2 replies
  • 0 kudos

Looking for documentation to create custom boards in STM32 Motor Control Software Development Kit (MCSDK) 6.1

Hi,these days you released STM32 Motor Control Software Development Kit (MCSDK) 6.1 which offers the possibility to create custom boards. The sample boards are very complex and the code is very long. I'm looking for documentation how to write a custo...

froesel by Associate III
  • 2701 Views
  • 2 replies
  • 4 kudos

Resolved! Debugging problem

Dear sir, We are working on one of our pharma project in which we want to drive a hall-sensored BLDC motor  using x-nucleo-ihm08m1 board. So we've downloaded firmware provided by ST microelectronics (STM32CubeExpansion_SPN8_V1.0.2) in which we are lo...

vishu by Associate II
  • 9402 Views
  • 9 replies
  • 1 kudos

Resolved! problem in STM32Cubeide

Hello,Im new to this and im stuck on 2 things i generated a code from the motorcontrol workbench and im using a Nucleo 64 f030R8 with a IHM07M1A BLDC Motor controller. i can start the motor and control speed. 1st question : where can i change directi...

Resolved! DMA and OC MODE

 Hi,1. Project Purpose:  Generate pulse to control stepper Driver. 2. My method and step:  1) every 2 milisecond calculate out the pulse need to send next cycle;  2) DMA and Timer Handle the pulse sending.      a. Timer update interru  3pte cycle is ...

Nickle by Associate
  • 2432 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.