STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Details about Motors with stm32f429zi

Hi,I am new to this community. I want suggestion regarding, going to do the setup of two-axis gimbal with Nucleo stm32f429zi and two gdm4108 motors. Is this setup will work?What are all things to cover?Regards,Kamalesh

kamalskdy by Associate II
  • 3224 Views
  • 8 replies
  • 0 kudos

ST motor profile issues in connection

Hi All, I met some issues in ST Motor profile. It showed me waning as below when i click connect.I am sure that serial port was not used by others.I flashed a uart sw and it can work normally.My control board is Nucleo G431RB, power board is X-NUCLEO...

Ddew1_0-1733319566260.png Ddew1_1-1733320008632.png Ddew1_2-1733320588301.png
Ddew.1 by Associate
  • 758 Views
  • 0 replies
  • 0 kudos

MC FOC Motor Control Workbench

Hello everyone,I would like to understand about MC library and some motor control terms. 1 - I want to use my own power board and motor. In this case, how can I specify the PID and motor parameters using MC workbench.2 - is auto tuning available in t...

Zek_De by Senior
  • 851 Views
  • 0 replies
  • 0 kudos

Unable to turn the start/stop button on MCSDK

Tools : MotorControl Workbench_6.3.0, CubeMX_6.12.0, CubeIDE_1.15.0Issue : The start/stop button is configred in .stwb6 as attached but this button does not shown in "User Interface"  and "Pin Usage & HW Changes"tab. I tried to generate the project t...

SJ_JG by Associate
  • 1072 Views
  • 1 replies
  • 0 kudos

HSO recommended hardware setup

Hi,While reading the "HSO Startup Guide" included in the release notes of Motor Workbench 6.3.2, I came across a recommendation regarding the filtering of voltage: This raised the following question: considering that the only development kit offered ...

RTirapegui_0-1732923108675.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.