STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Minimum programming configuration for STSPIN32G0601

I have attempted to interface an STSPIN32G0601 using only connections to an ST-LINK (V2).  That is: there are no other connections to the target IC other than SWCLK to PA14 (pin 62), SWDIO to PA13 (pin 61), GND to VSS (pin 8), and 3.3V to VDD (pin 7)...

FMadi.1 by Associate III
  • 2412 Views
  • 4 replies
  • 0 kudos

Resolved! Installation error of FP-IND-DATALOGMC

STM32CubeFunctionPack_DATALOGMC_V1.1.1をwebからダウンロードし Downloaded STM32CubeFunctionPack_DATALOGMC_V1.1.1 from the web. en.fp-ind-datalogmc\STM32CubeFunctionPack_DATALOGMC_V1.1.1\Utilities\HSDPython_SDK\HSDPython_SDK_install.batを実行すると When I run en.fp-i...

hamaogeoge_1-1731919803763.png hamaogeoge_0-1731919726745.png

Motor Pilot bug: Torque resets to zero

I'm having following issue with the Motor Pilot that comes with the MCSDK 6.2.1 (V1.2.5).I try to modify the Rev-up phase configuration.Now when I write a torque value in any of the phases, this value resets to zero and is saved on the board (pressin...

DMeie.2 by Senior II
  • 7431 Views
  • 15 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.