2024-12-09 5:16 PM
I want to create a project with the Motor Control library using CubeMX.
However, The Motor Control library is not registered as a software package in CubeMX, Now.
Refering some application note, it says to use CubeMX's X-CUBE-MCSDK, but this software package is not available in CubeMX.
I wonder if the X-CUBE-MCSDK software package will be available again in the future.
Solved! Go to Solution.
2024-12-10 2:04 AM
Hello just4u78,
You are right, the MCSDK is not available as a CubeMX package. This may be subject to discussion in the future but there is currently no plan to make it part of it. You can still use the MCSDK as a standalone tool, that calls CubeMx whenever generation is needed.
2024-12-10 2:04 AM
Hello just4u78,
You are right, the MCSDK is not available as a CubeMX package. This may be subject to discussion in the future but there is currently no plan to make it part of it. You can still use the MCSDK as a standalone tool, that calls CubeMx whenever generation is needed.
2024-12-10 2:26 AM
I don't understand why this library was excluded from the software pack.
In the current situation, if I want to create a new MCU board with the MC library, I must either create a new board in MCWorkbench board manager tool and use it, or configure the project manually.
I want to create an MCU board that can only give commands like Motor Pilot.
(You called it a Performer Device in Motor Control Protocol Suite Manual)
I want to say that "It's not easy for a beginner to set it up through the Board Manager".
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.