STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

L6480HTR Current problem

We are operating the motor with the Run command “Run(DIR, SPD)” to rotate it at a constant speed. However, when the speed (SPD) is varied and then returned to the same SPD, we observe a significant increase in current.We send the Run command to the d...

TOAMUSEN by Associate
  • 718 Views
  • 0 replies
  • 0 kudos

Torque mode speed limiter

Hello everyone,How can I set a speed limiter when I use the motor in Torque Mode(FOC)?. I am getting an oscillation.I am using St motor control workbench.In addition, motor in speed mode , when I apply a less speed then I am getting the motor in zero...

Zek_De by Senior
  • 994 Views
  • 0 replies
  • 0 kudos

Resolved! Hardware design file

Hi,I am looking for hardware reference design source files for STEVAL-ESC002V1 board.Is it available to speed up the design activity?Thank you for your kind attention and immediate response Sincerely,Raj 

SPI communication of L6482

Hello, I encountered some issues while using SPI to control L6482:1. My read/write SPI logic seems to have failed, unable to read/write normally. Is this a problem with my SPI timing?This is the timing sequence for me to retrieve the status register....

lcc1111_2-1735090518149.png lcc1111_3-1735090550487.png
lcc1111 by Associate
  • 609 Views
  • 0 replies
  • 0 kudos

Dead Time between different channels

I want to configure dead time between different channels but I get the output as in the picture.Below is the PWM function I created for the BLDC motor and algorithm for each phase of BLDC motor. What could be the problem?  void BLDC_SetPhase(uint8_t ...

BLDC_logic.png PWM.jpg

Resolved! can't connect Motor Profiler to Nucleo-L476RG

Hello,i am beginner in ST motor control domain.I have installed the following software versions :MC workbench v6.3.2CUBE IDE v1.16.1CUBE MX v 6.12.1I have a problem when trying to connect my board using profiler. In log, i can see the last two messag...

Thierry81 by Associate II
  • 2159 Views
  • 4 replies
  • 0 kudos

Hall Sensor in Steval IPM 30B

I am trying to control BLDC motor with Steval IPM30 B and Nucleo L476RG as controller. In sensor less mode it is working fine but when I am using Hall Sensor it is not rotating at all and its showing speed feedback error at the starting only. How to ...

Screenshot 2024-12-03 122241.png
hu88 by Associate II
  • 3218 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.