STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Startup failure without mechanical load

Hello,we are using Sensorless FOC with open loop starting of the BLDC motor. The Motor is starting reliably under normal and heavy load conditions. But without load the I got startup failure. Any idea what paramter should be checked or improved?MC SD...

RReic.2 by Associate II
  • 846 Views
  • 1 replies
  • 0 kudos

Resolved! STM Motor Control WorkBench

Hi, I have installed MC WorkBench(6.3.2). While Project Generation it gives "STM32CubeMX not found" error. I have already installed STM32CubeMX (6.14.1), also STMCube IDE (1.2.1).Is there any setting that needs to be done?Thanks,Harsh 

Harsh_M_0-1747651024987.png
Harsh_M by Associate II
  • 1302 Views
  • 2 replies
  • 0 kudos

Code generation fail in the MC workbench

Hi, I have a project in the MC workbench and I can generate code (for stm32F407) successfully when I use the "Three Shunt Resistors" current reading topology, and the code works well on my board. Now I need to change my board and use the current sens...

post1.jpg post2.jpg post3.jpg post4.jpg
DF_MC by Associate III
  • 1878 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 ZEST Kit & Motor Control Workbench 6.2.1

Dear Sir or Madam,I tried to generate code for the STM32 ZEST Kit consisting of trying to evaluate HSO (while waiting for ZEST approval):1) STEVAL-LVLP012) B-MOTOR-PMSMA13) B-G473E-ZEST1SSince the motor (2) is not available I tried using the Motor Pr...

MoCo by Associate II
  • 11261 Views
  • 11 replies
  • 3 kudos

Resolved! brake function in 6-steps

Hello,I am currently designing an ESC for a small vehicle (around 300g).  I made a first proto board and I use the 6-steps algorithm with an hall sensored motor. I would like to be able to brake. I firstly thought to short all the phases directly to ...

Xavier75 by Associate II
  • 2357 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.