STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! How to configure the motor open loop mode?

hello everybody:    l'm currently debugging the FOC motor with MC Workbench. Now I have generate the code with the open loop configuration. According to the user mannual, I can use the APIs in the code as follows:------------------------------------F...

DF_MC by Associate III
  • 956 Views
  • 3 replies
  • 0 kudos

How run motor using PWM in STSPIN32F0A

I have a STSPIN32F0A board on which, I need support on below points1) Ability to operate the motor through LIN/PWM signal rather than an ADC signal, currently the EVAL board supports an ADC through an onboard potentiometer which I want to remove. 2) ...

HSing.5 by Associate II
  • 846 Views
  • 1 replies
  • 0 kudos

Firmware error for motor profiler

 I am using the Nucleo-IHM17M1 and Nucleo-F401RE to evaluate a high-speed drone motor (22,000KV) with sensorless drive. I am particularly interested in the Motor Profiler function, since some key motor parameters are not provided by the manufacturer....

STM.png
uskach by Associate
  • 1012 Views
  • 4 replies
  • 2 kudos

ACIM MOTOR SPEED CANNOT INCREASE

 I can't increase the motor speed beyond a certain point.For example, when using the ST Motor Pilot interface, I set the Speed Reference variable to 2500 RPM, and the Mechanical Speed reaches approximately the same value (2495 RPM). However, when I i...

Omer Ab by Associate III
  • 4861 Views
  • 18 replies
  • 1 kudos

Resolved! Extern Potentiometer MCSDK

Hello,I bought the STM32 Nucleo Pack with the Nucleo-F302R8, the X-Nucleo-IHM07M1 and a three-phase motor.I use MCSDK to control my motor and it's no problem.But when I want to add an external potentiometer to the ADC, I can't get the values from it....

Resolved! VNH707AY motor driver interface with STM32

Hello All,I'm using VNH707AY motor driver to drive 2 motors separately i want to interface with my STM32Can anyone share the schematic or  references for the same which can help me in this.Thanks & Best Regards,Sakshi 

sakshi by Associate III
  • 749 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.