STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Safe Limited Speed with STM32 microcontroller

Hello I am working on a 48V BLDC drive unit and I would like to implement the safety feature "Safe Limitd Speed" according SIL2/3 and PLc/d.In the Motor Control Reference Guide from ST there is "Safety ready: SIL, Class B" as one of the key features ...

PBlat.1 by Associate
  • 1414 Views
  • 1 replies
  • 0 kudos

Stm32 ADC trigger at certain time

Hello friends, i want to read ADC value for particular time. That is, to read the analog value during the middle time of every pwm signal. Triggering ADC via timer.I had generated pwm signal with 50% duty cycle in center align mode so that we could e...

0693W000003RYOXQA4.png
Bud by Associate III
  • 3959 Views
  • 4 replies
  • 0 kudos

Resolved! BLDC back emf problem using Motor Work Bench

We're in the process of designing BLDC motor controller for solar pump (1HP and 2HP), we plan to use `STGIB15CH60TS` IPM to drive motor and `STM32F103RC` as controller. We started design using `MotorControl Workbench 5.4.4`, however in this we are no...

snair.1 by Associate
  • 1403 Views
  • 1 replies
  • 0 kudos

STM32F303CB Motor control setup can't avoid stalling

Hi,I am using the STEVAL-ESC001V1 development kit board with a BlueRobotics T200 motor. The motor runs well with the provided SDK firmware and the motor profiler values, but we are having a couple of issues when changing speeds:The range of the poten...

ASilv.8 by Associate
  • 1931 Views
  • 3 replies
  • 1 kudos

Resolved! Encoder feature in STM32F070CB

Hello,I need a help in Motor frequency calculation with more precision. I am using STM32F070CB for my application. My requirements are1) Monitor the Motor frequency based on quadrature pulses.2) If Frequency varies by +/-15%, need to process some saf...

MSatish by Associate II
  • 3193 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.